MCF52xx / CW6.2 / Feescale USB Wiggler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52xx / CW6.2 / Feescale USB Wiggler

2,476件の閲覧回数
jhh29
Contributor I
Hello,
 
Can anyone confirm if the new  Freescale USB Wiggler will support MCF52xx devices in CW6.2 , when released?
 
Best Regards
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

914件の閲覧回数
DistiCasMgr
NXP Employee
NXP Employee
The new Freescale Wiggler being USB-TAP?
In which case YES it will support the 52xx devices BUT not until V6.3 which is in Alpha test right now.
0 件の賞賛
返信