Hi,
I'm trying to program NAND flash from scratch for T1024RDB Rev C Evaluation Board. CW version is 10.5.1. I compiled 't1024-core00 for SRAM' and tried to debug the code with 't1024-core00_SRAM_T1024_Download' configuration using CWTAP ethernet, but Code Warrior throws following error "CCS Protocol Plugin: Failed to correctly configure JTAG chain" .
I tried configuration with ..\PA_Support\Initialization_Files\jtag_chains\T1024RDB_RCW_1400_1600.txt, but it didn't work too.
CCS log is in the attachment.
Could anyone help me?
Original Attachment has been moved to: T1024RDB.txt.zip
Solved! Go to Solution.
Please set the board to hardcoded rcw 010011011 (SW1 + SW2[1]) - where 0 is ON, open the ccs.exe from \Freescale\CW_PA_v10.5.1\PA\ccs\bin\, use the following command and provide the output:
delete all
config cc cwtap
ccs::config_chain t10xx
ccs::reset_to_debug
Adrian
Please set the board to hardcoded rcw 010011011 (SW1 + SW2[1]) - where 0 is ON, open the ccs.exe from \Freescale\CW_PA_v10.5.1\PA\ccs\bin\, use the following command and provide the output:
delete all
config cc cwtap
ccs::config_chain t10xx
ccs::reset_to_debug
Adrian
Please provide the switch settings from your board.
Adrian
SW1 = 0001 0011
SW2 = 1011 1111
SW3 = 0010 0001
where 0 is ON
Ttry to set the board for NOR boot, then try to flash the NAND device.
Adrian
Nothing changed
Hello
The error message shows core is not in good state. You may try to use Hard-coded RCW by switch setting. SW1[1...8]SW2[1]: 010011011, and try again.
Error message: T1020: Core not responding
Regards
Lunmin