IRQ Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IRQ Interrupt

跳至解决方案
2,707 次查看
polofermin
Contributor III

Hello,

I am new in CodeWarrior:

-I am targeting with MCF51EM256 CPU

-My version of CodeWarrior is: Codewarrior IDE version 5.9.0 Build 2830

I´m programming with FreeRTOS kernel and I use IRQ interrupt. I don´t have any problem with linker, but when I simulate the program entry for once in the IRQ interrupts and it doesn´t entry again (also I erase IRQ flag to entry in the interrupt)

any idea?

 

Thanks so much..

Best regards 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,474 次查看
polofermin
Contributor III

I already know why the interrupt was not working ... I was erasing the IRQ settings register, and I just had to clear the ACK bit (only)...thank so much

BYe!

Best regards and merry christmas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,474 次查看
tkvenki
Contributor III

Hi,

 

It will be better if you can be more descriptive.

Is it a sample code you are running, or your custom application....

Which target are you running??....SDRAM/SRAM/ROM??

What do you mean by simulating program entry??

 

Also it will be better if you can  post your

1. LInker.

2. CFG file

3. vector.s file...

 

because, if it is a start-up problem, 

these are the popular suspects...

 

Regards,

Venki

0 项奖励
回复
1,475 次查看
polofermin
Contributor III

I already know why the interrupt was not working ... I was erasing the IRQ settings register, and I just had to clear the ACK bit (only)...thank so much

BYe!

Best regards and merry christmas

0 项奖励
回复