How to generate .a2l file from codewarrior .map file?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to generate .a2l file from codewarrior .map file?

ソリューションへジャンプ
9,732件の閲覧回数
hbch
Contributor III
I am using codewarrior for MPC55xx V2.4 and the target is MPC5633m. The .map file generated by the linker can not be converted to .a2l file by Vector ASAP2 Editor which is a tool of CANape. Can anyone help me?
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
5,305件の閲覧回数
hbch
Contributor III
I am sory to report that the solution does not work at all. The A2l misses variables' names and their addresses. If in standard format, the a2l file can get the variables' names but no addresses. Please refer to the attached file.
Message Edited by hbch on 2009-07-23 12:50 PM

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,470件の閲覧回数
puliufeng
Contributor I

I met the same problem,how to slove it?  Need help

0 件の賞賛
返信
5,305件の閲覧回数
ronco
NXP Employee
NXP Employee

We haven't used the Vector ASAP2 Editor before but we just installed a demo and the only suggestion we have is to set the  MAP file definition  to Metrowerks.  Take a look at the attached screenshot for an example.  I hope this helps.

 

-Ron

0 件の賞賛
返信
5,306件の閲覧回数
hbch
Contributor III
I am sory to report that the solution does not work at all. The A2l misses variables' names and their addresses. If in standard format, the a2l file can get the variables' names but no addresses. Please refer to the attached file.
Message Edited by hbch on 2009-07-23 12:50 PM
0 件の賞賛
返信