How to enter a "Custom" configuration value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enter a "Custom" configuration value

3,301件の閲覧回数
danmoffatt
Contributor II

What procedure is required in order to be able to enter a Custom configuration value in the CodeWarrior TAP tool PBL component as opposed to selecting one of the drop down menu items?

I have done it in an old LS1088A project but I forget the procedure/syntax to incorporate it in a new project that I am currently working on.

PBL Custom Value.PNG

0 件の賞賛
返信
7 返答(返信)

3,272件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I installed CodeWarrior for ARMv8 11.5.12, and found there was no option for "0b10 Custom value".

In your IDE, you could select "skip error checking" to continue your configuration.

yipingwang_0-1675845975794.png

 

0 件の賞賛
返信

3,265件の閲覧回数
danmoffatt
Contributor II

Thank you for your reply.

Yes once the custom value is entered then you have to skip error checking in order to build the code.

The real issue is that the CodeWarrior tool has a fault in that it provides the RCW bits 212-211 binary setting as 0b01 for selecting the System Clock as the DDR_REFCLK_SEL.  The correct binary setting is 0b10 and hence a custom value needs to be entered in the tool settings.

danmoffatt_0-1675864755768.png

 

0 件の賞賛
返信

3,252件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It seems that this is a defect of CodeWarrior for ARMv8 11.5.12, I have reported this defect to QCVS PBL tool development team.

0 件の賞賛
返信

3,296件の閲覧回数
KalaimaniArumugamdev
Contributor III

Hi @danmoffatt 

Refer "QCVS PBL Tool User Guide" chapter " 1.1.1.2.1 Specifying custom values".

 

Thank

Kalaimani Arumugam 

0 件の賞賛
返信

3,261件の閲覧回数
danmoffatt
Contributor II

Hi

Unfortunately, the "Ignore Constraints and non-critical Errors" option is not selectable for me (i.e., it is "greyed" out).

0 件の賞賛
返信

3,289件の閲覧回数
danmoffatt
Contributor II

I have downloaded the document and will give it a try.

Thank you very much!

0 件の賞賛
返信

3,287件の閲覧回数
KalaimaniArumugamdev
Contributor III
Great
0 件の賞賛
返信