How to add OSBDM for MCF51ACxxx in CW for Microcontroller V6.3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add OSBDM for MCF51ACxxx in CW for Microcontroller V6.3?

Jump to solution
2,584 Views
bluehacker
Contributor III

HI, everyone!

 

Recently, I develop one MCF51AC128 project, when I create project in cw for mcu v6.3, if  I select target MCU as MCF51AC128, the OSBDM-JM60 item don't appear in "choose your default connection". (see attachment)

but if I select MCF51CN128 as my target MCU, the item appears.

My queation is How to add OSBDM-JM60 item into cw for MCF51AC128?

 

 

thank you

Labels (1)
0 Kudos
Reply
1 Solution
1,640 Views
stanish
NXP Employee
NXP Employee

Hi bluehacker,

 

You can select the FSL Open Source BDM connection interface directly from the debugger:

The Debugger menu "Component" -> "Set Connection" -> Processor: COLDFIRE; Connection: "FSL Open Source BDM"

See attached screenshot.

 

Stanish

 

 

View solution in original post

0 Kudos
Reply
4 Replies
1,641 Views
stanish
NXP Employee
NXP Employee

Hi bluehacker,

 

You can select the FSL Open Source BDM connection interface directly from the debugger:

The Debugger menu "Component" -> "Set Connection" -> Processor: COLDFIRE; Connection: "FSL Open Source BDM"

See attached screenshot.

 

Stanish

 

 

0 Kudos
Reply
1,640 Views
bluehacker
Contributor III

thanks for you

0 Kudos
Reply
1,640 Views
bluehacker
Contributor III

It is so morose, I find cw for mcu v6.3 and v10.0 can't support mcf51acxxx. it always indicates can't connect with MCU

I use OSBDM-JM60, does this BDM don't support MCF51ACxxx?

 

0 Kudos
Reply
1,640 Views
pgo
Senior Contributor V

Dear bluehacker,

 

Would this thread be relevent?

 

https://community.freescale.com/message/63749#63749

 

bye

0 Kudos
Reply