Help to use Code generated by RAppID-MPC5554 in CW MPC55xx V2.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help to use Code generated by RAppID-MPC5554 in CW MPC55xx V2.2

2,009 Views
n_
Contributor II
I use Rapid Application Initialization and Documentation Toll (RAppID) for MPC5554 to generate Code. But when I create new MPC5554's project and add these codes, There are many Errors. I have tried using RAppID to generate code for 3 different compilers (Metrowerks, Diab, GreenHills), but there are still many errors and the errors are different.
Please guide me to use Code that generated by RAppID-MPC554 in CodeWarrior.
Thanks,
     
Labels (1)
0 Kudos
Reply
1 Reply

964 Views
Voxan
Contributor III
Hi there,

I would guess Rapid is not generating standard C code, that may explain different errors using different compilers.

Back to your issue, I'm afraid you will have to investigate errors one by one and adjust settings/configurations accordingly.

Hope this helps...

Regards
0 Kudos
Reply