Help to use Code generated by RAppID-MPC5554 in CW MPC55xx V2.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help to use Code generated by RAppID-MPC5554 in CW MPC55xx V2.2

2,084件の閲覧回数
n_
Contributor II
I use Rapid Application Initialization and Documentation Toll (RAppID) for MPC5554 to generate Code. But when I create new MPC5554's project and add these codes, There are many Errors. I have tried using RAppID to generate code for 3 different compilers (Metrowerks, Diab, GreenHills), but there are still many errors and the errors are different.
Please guide me to use Code that generated by RAppID-MPC554 in CodeWarrior.
Thanks,
     
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,039件の閲覧回数
Voxan
Contributor III
Hi there,

I would guess Rapid is not generating standard C code, that may explain different errors using different compilers.

Back to your issue, I'm afraid you will have to investigate errors one by one and adjust settings/configurations accordingly.

Hope this helps...

Regards
0 件の賞賛
返信