Help!!! Can I use bdiCW to program the on board flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help!!! Can I use bdiCW to program the on board flash

1,594件の閲覧回数
forums_frank
Contributor I
Hello,
We are going to develop our new products based on coldFire MCF54452 processor and also considering CodeWarrior as the development environment. We also want to buy the bdiCW from ABATRON as our BDM/JTAG interface.

Can we use bdiCW to program on board flash? There is nothing about this feature in the production spectification.

Cheers
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

631件の閲覧回数
J2MEJediMaster
Specialist I
You might just want to download the Special Edition of CodeWarrior (it's free), and try looking at the supported debugger connections. To do that:

1) Launch CodeWarrior.
2) Go to the Project Settings panel by typing ALT F7.
3) Under the Target Setting Panels choices in the column on the left, pick Remote Debugging.
4) In the Remote Debugging panel that appears, go to the Connection options drop-down menu and examine the choices there. I see choices for Abatron TCP/IP and Abatron serial, but I don't know if those are suitable for the Abatron part you're talking about.

Fair warning: the Special Edition download is pretty big (over several hundred megabytes), but it may give you the opportunity to check out features on the toolset that you might have questions about. HTH.

---Tom
0 件の賞賛
返信