I am using CodeWarrior 10.0.7 in Windows7 system. I started the new project from CodeWarrior Baseboard Project Wizzard and connecting a TWR-LS1021A to the CodeWarrior TAP via USB. When I tried to debug, it connects, but no source code shows up? I used to see the main() and be able to step thru the code, but now, I don't see any source code, instead getting this error message:
"No source available for "0x00000000 (0x00000000)() ""
Any idea, what is missing?
Thanks
Jey
Solved! Go to Solution.
Hi Jey Surier,
See the difference between attach, connect and download:
https://community.freescale.com/thread/331574#470672
Regards
Lunmin
Hi Jey Surier,
See the difference between attach, connect and download:
https://community.freescale.com/thread/331574#470672
Regards
Lunmin
Hi Jey,
From what I see in your image, you have used Connect launch, Connect will run init file, will reset the board, but will not download code into the board. For doing debug to bareboard project you have to use Download launch.
Adrian