Hi,
Now, I used the Flash Programming software in the codewarrior to flash the internal flash.
Below are the settings in the Flash Programmer software:
Target Configuration:
=====================
Target Initialization: Used the file MCF5282C3_PnE.cfg
Target RAM Memory Buffer: 0x00000000 , Size = 0x00006000
Flash Configuration:
====================
Flash Memory Base Address: 0xF0000000
Device: M5282_CFM
Program/Verify:
===============
Selected file (The S19 file that i generated)
Restrict Address Range from F0000000 to F007FFFF.
I am able to erase the Flash contents and Program successfully.
When i Debug (in codewarrior) it goes to the starting location of asm_startmeup, but the data is junk (00000000) in that.
And then it jumps to asm_exceptionhandler.
So, i went to the dBug prompt and said go 0xF0001118 (Which was the starting location it showed when i said debug in prev step).Iam able to execute the application.
I have the following questions.
1. Any reason, why i am not able to debug in code warrior.
2. If i need to boot from the internal flash, what should i do? I set the SW1-8 and 9 to OFF (Internal 32-bit) and restarted the evaluation board, the execution must have started. It did not happen.
3. Any jumper settings need to be done?.