As title, does CW PA v10.3 support t1040 boards?
I can only create Codewarrior Bareboard project for QorIQ P1/P2/P3/P4/P5 T4 boards, what about T1 series?
I want to debug my T1040qds, but I'm not able to create a project for T1 series.
Solved! Go to Solution.
The case has been closed, please raise a new case to get the answer.
Thanks.
Please use NXP CodeWarrior 10.5.1 to create T1 series project.
Hi June,
Thanks for your reply, I have a follow-up question, when I create an attach configuration it seems that the 10.5.1 doesn't support the use of USB TAP for t1040qds. I can only select CodeWarrior TAP (over USB), CodeWarrior TAP (over eth), Gigabit TAP or Gigabit TAP +Trace. While for t2080, I can select the Connection Type as USB TAP. I only have a USB TAP debugger. Is there a version that supports the use of USB TAP debugger on t1040?
BRs
Minghu.