Coldfire: Q on latest CodeWarrior Special Edition debug support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coldfire: Q on latest CodeWarrior Special Edition debug support

3,390件の閲覧回数
Harjit
Contributor II
Does it support Coldfire with the ICD Cable. The ICD cable is a BDM cable that plugs into the parallel port and has a 10 pin connector (0.1", 2x5).
 
I use this with SingleStep and a 68376 and wanted to know if I could use this cable on a MCF5212 design.
 
Also, does CodeWarrior Special Edition come with a ROM based monitor that I can use with CodeWarrior so that I can debug over the serial port?
 
Thanks,
Harjit

Message Edited by CrasyCat on 2007-04-13 11:30 AM

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,884件の閲覧回数
Harjit
Contributor II
Thank you for the information.
 
The reason I am looking for a serial ROM monitor is that I want to use a Coldfire part on a robot.
 
With BDM, if I am single stepping, it stops the processor to read the Addr/data registers. This will wreak havok on my servo loops.
 
When I am using a serial ROM monitor, I can set the servo loop interrupt level to be higher level than the serial ROM monitor so I can do source level debugging as well as have the servo loop running. I have this running on a 68376 based system and it works quite well.
 
Regards.
0 件の賞賛
返信

1,884件の閲覧回数
CrasyCat
Specialist III
Hello
 
  For CW Coldfire we support following P&E interface cable:
       - Cyclone Max
       - USB-ML-CFE
       - BDML-CF
       - BDML-CFLV
       - CABLE-CF
The cable used for debugging on CPU32 (68376) cannot be used for debugging on Coldfire. You need another cable.You need a 26-pin connector on the board.
 
There is no ROM monitor connection available in special edition.
 
CrasyCat
0 件の賞賛
返信

1,884件の閲覧回数
Harjit
Contributor II
Thank you for the prompt response.
 
Can you tell me which version of CodeWarrior includes the ROM monitor?
 
I thought I read documentation that said that I could get away with a 10 pin connection on Coldfire processors for BDM. Am I mistaken? This is a concern because my board won't have space for the 26 pin connector...
 
Thanks,
Harjit
0 件の賞賛
返信

1,884件の閲覧回数
CrasyCat
Specialist III
Hello
 
BDM connector layout is defined by the hardware and as far as I know the connector for Coldfire is 26 pins.
 
I do not think you can debug/connect to a Coldfire board without the standard BDM connector.
 
We do not have ROM monitor available for debugging on Coldfire.
If you are looking for a low cost debug solution, you may want to look into following Post from the Coldfire Forum: http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=624
 
This may be working for you too.
 
CrasyCat
0 件の賞賛
返信