CodeWarrior is free available for QorIQ Qonverge Platform?

cancel
Showing results for 
Search instead for 
Did you mean: 

CodeWarrior is free available for QorIQ Qonverge Platform?

295 Views
Contributor I

Hi all,

 

I am trying to create a new project for QorIQ Qonverge just to try the CodeWarrior tool and evaluate how difficult would be to develop an application on that platform. I have downloaded the CodeWarrior Development for Power Architecture v10.1.1 and the SP1 update. However, when following the tutorial CodeWarrior for Power Architecture Processors - Quick Star, the option QorIQ Qonverge doesn't appear among the list of processors and do appear in the tutorial.

 

Did I miss something? Is it possible to use CodeWarrior Developmente IDE for QorIQ Qonverge PSC9130 in a free trial?

 

Thank you

Labels (1)
0 Kudos
2 Replies

34 Views
Specialist I

Support for the PSC9131 in CodeWarrior for PA V10.1 is made available through the installation of a limited-distribution service pack. You can check this https://community.freescale.com/message/103430#103430, but the short answer is you need to contact your Freescale representative to obtain this service pack.

 

---Tom

0 Kudos

34 Views
Contributor I

Thank you

0 Kudos