Cannot find CONFIG_CW_DEBUG option in kernel configuration for T4240RDB sdk.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot find CONFIG_CW_DEBUG option in kernel configuration for T4240RDB sdk.

3,024 Views
saqlain_raza
Contributor I

Hi everyone,

Previously we have been enabling CONFIG_CW_DEBUG option in the Kernel config when doing Linux kernel debugging on T4240RDB board using NXP CodeWarrior TAP. But now in the latest QoriQ SDK I am unable to locate this option in the kconfig file.

Has this option been removed ? If so, is there any alternative option that I need to enable for kernel debugging.

 

Thanks...

Labels (1)
0 Kudos
Reply
3 Replies

2,807 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Saqlain Raza,

The option CW_DEBUG is not needed in SDK 2.0 release, because CW_DEBUG is only required by e500v2 platforms, but e500v2 platforms have already been removed from SDK 2.0.


A short overview:

for e6500: you can debug the target with CW_DEBUG disabled, except the case where the target enters in idle mode    (PW20 state I guess). From this state, due to HW design limitation, you can not use external debug.Therefore, if there is a way to disable this state from Linux, you should be able to debug e6500 without CW_DEBUG.

for e500mc and e5500: you can fully debug the target with CW_DEBUG disabled.

for e500v2: you must use CW_DEBUG to enable external debug flags from MSR. There no way you can Debug with probe without these flags set.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,807 Views
saqlain_raza
Contributor I

Hi Yiping,

Thanks for the response. Do you have any recomendation about how the idle mode for e6500 can be disabled in Linux kernel ?

Regards..

0 Kudos
Reply

2,807 Views
saqlain_raza
Contributor I

Hi Yiping,

When debugging SMP kernel with SDK 2.0 (i.e without CW_DEBUG) the debug session does start but resuming the target after a brekpoint hit or sometimes randomly doesn't resume the target . Though the debug session seems to be active however the target's serial console/terminal is not resumed. On suspending the target execution the debugger shows that most of the cores are executing in arch_spinlock routines.

Can you suggest that how the idle mode for e6500 cores can be disabled in the Linux kernel ? I do see some code

inside the idle task in arch/powerpc/kernel/idle.c . Is that the correct place to look into ?

0 Kudos
Reply