Cannot Connect to LS1020A with QorIQ DDR Validation Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot Connect to LS1020A with QorIQ DDR Validation Tool

Jump to solution
1,889 Views
perfranck
Contributor III

Hello.

 

We are trying to validate our DDR4 settings on a custom LS1020A board, following the guides for the DDR Validation tool for the qoriq configuration in codewarrior. (http://cache.freescale.com/files/soft_dev_tools/doc/user_guide/QCVSDDRVGETSTARTUG.pdf )

 

In this guide, step 1.4, we are unable to connect to the hardware

We get a broken link next to the Target drop-down with the tooltip: Target is not ready: target does not respond and/or could not be reset.

 

We are using the CWTAP with USB / Ethernet connection, and we can debug programs on the system fine.

 

Our target settings are:

Processor: LS1020A

Probe Type: CWTAP

Target Access: CDDE

Probe Address: <mac address of CWTAP or IP Address of CWTAP or Blank>

JTAG Clock Speed: default (have tried a few different ones)

 

We are suspicious that this is due to the ARM not being alone on the JTAG chain, we have a Xilinx part in front of the ARM and our JTAG Config File for debugging program has:

 

Generic 6 1 0x3f

LS1020A <...>

DAP

SAP2

 

Any ideas?

Labels (1)
0 Kudos
Reply
1 Solution
1,016 Views
addiyi
NXP Employee
NXP Employee

Because in this moment QCVS tool doesn't provide an option for customize the jtag chain and changing the test script could be used as workaround. For this go to eclipse\Optimization\resources\QorIQ\common\templates\init\ and edit:

connect.py, connect_to_target function:

cpuVariant = [ [6, 1, 0x3F], "LS1021A" ]

connect_call.py:

cpuVariant = [ [6, 1, 0x3F], "LS1021A" ]

After that, restart CW/eclipse.

Adrian

View solution in original post

0 Kudos
Reply
4 Replies
1,017 Views
addiyi
NXP Employee
NXP Employee

Because in this moment QCVS tool doesn't provide an option for customize the jtag chain and changing the test script could be used as workaround. For this go to eclipse\Optimization\resources\QorIQ\common\templates\init\ and edit:

connect.py, connect_to_target function:

cpuVariant = [ [6, 1, 0x3F], "LS1021A" ]

connect_call.py:

cpuVariant = [ [6, 1, 0x3F], "LS1021A" ]

After that, restart CW/eclipse.

Adrian

0 Kudos
Reply
1,016 Views
perfranck
Contributor III

Thanks for your reply, Adrian.

I changed the file /opt/Freescale/CW4NET_v2016.01/Common/QCVS/Optimization/resources/QorIQ/common/templates/init/connect.py and /opt/Freescale/CW4NET_v2016.01/Common/QCVS/Optimization/resources/QorIQ/common/templates/init/connect_call.py to include the changes as listed below. however, i see this in CCS.

CCS output

loading history file ... 48 events added

CodeWarrior Connection Server console display active (Tcl8.4.6 / Tk8.4.6)

Loading CCSAPI Tcl interface (/opt/Freescale/CW4NET_v2016.01/Common/QCVS/Optimization/target-connection/cdde/ccs/bin/ccstcl.so)...

Loading Svfburner (/opt/Freescale/CW4NET_v2016.01/Common/QCVS/Optimization/target-connection/cdde/ccs/bin/svfburner.so)...

CC config string is invalid

Server listening on port: 41475

Server listening on port: 50000

Clients allowed from all hosts

No clients denied

CCSAPI connection #1 accepted from localhost at Tue May 31 08:31:05 2016

CCSAPI connection #1 from localhost closed at Tue May 31 08:32:25 2016

And the connection fails. I have three connections in codewarrior, one with the CWTAP id left blank (should use USB), one with the MAC address of the device, and one with the IP address of the device. Each one will report "Connection script timed-out! Please verify that the target and target probe are connected and configured correctly."

connect.py

...

    tcf.show_info(False)

    # Workaround for our JTAG chain, which has a Xilinx part on it

    cpuVariant = [ [6, 1, 0x3F], "LS1021A" ] 

    # Workaround for LS102x connectivity, that needs a special target name format. Example: [['LS1020', 'Rev1']] instead

    # of 'LS1020'.

    if cpuVariant in armv7_devices and majorRev == 1:

        cpuVariant = [[cpuVariant, 'Rev1']]

    ccsPort = int(get_cmdline_argument(CCS_PORT_SHORT_ARG, CCS_PORT_LONG_ARG))

...

I'm wondering about the snippet about 'Rev1', if it will have impact on this situation here ... Our silicon is rev 2.0 iirc.

I tried with the workaround before and after the if block

connect_call.py

# Connect to CDDE

cddeConn = cdde.connect()

# Create a protocol instance and save it

p = cddeConn.p

# variables set from the software calling this script

cpuVariant = "<<{CPU_VARIANT}>>"

majorRev = <<{CPU_MAJOR_REV}>>

probeId = "<<{TAP_ID}>>"

jtagSpeed = <<{JTAG_SPEED}>>

checkBasicTargetOps = <<{CHECK_BASIC_TARGET_OPS}>>

# Workaround for our JTAG chain, which has a Xilinx part on it

cpuVariant = [ [6, 1, 0x3F], "LS1021A" ] 

# Connect to target

(conn, succeeded, reseted) = connect_to_target(p, cpuVariant, majorRev, probeId, jtagSpeed, checkBasicTargetOps, False)

if not succeeded:

    exit(-1)

Any ideas?

0 Kudos
Reply
1,016 Views
addiyi
NXP Employee
NXP Employee

Could you send a verbose log from ccs console (log v), when QCVS is trying to connect to the board?

Adrian

0 Kudos
Reply
1,016 Views
perfranck
Contributor III

CCSAPI connection #1 accepted from localhost at Wed Jun  1 10:50:13 2016

check_min_version(serverh=0,*version)

  api version: 00000004 00000006

available_connections(serverh=0,*count,*cc)

  connections: {0,73,0xa9feeefb}

cc_version(serverh=0,cc_index=0,index=1912679227,*version)

config_chain(serverh=0,cc=0,count=4,*devlist,*generic)

  devlist: unknown(0),ls1020a,dap,sap2

reset_to_debug(serverh=0,cc=0)

  ERROR(39): Subcore error encountered during multicore operation

parse_error_ext(coreh.{serverh=0,cc_index=0,chain_pos=0}, 39)

  error: LS1020A: Core not responding

CCSAPI connection #1 from localhost closed at Wed Jun  1 10:50:16 2016

0 Kudos
Reply