Can I get your help with a MPC564 and CW EPPC V8.7?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I get your help with a MPC564 and CW EPPC V8.7?

2,744 Views
CaoJason
Contributor I
Hi buddies:
 
   I am a new one to use freescale product.My lab have bought MPC564 and  CodeWarrior EPPC 5xx V8.7.But I don't know how to use them.Can you give me some advice?also can you provide "The Programmer’s Reference Guide for the PowerPC Architecture" to me?
  thanks a lot!
 
Jason Cao



J2MEJediMaster added MCU type and CW version to subject header
 


Message Edited by J2MEJediMaster on 2007-09-18 11:25 AM
Labels (1)
0 Kudos
Reply
2 Replies

468 Views
CaoJason
Contributor I
Thanks Master!
0 Kudos
Reply

468 Views
J2MEJediMaster
Specialist I
Try reading the docs that came with the installation for ideas how to start. The docs should be located in a Help directory folder in the CodeWarrior folder. You'll want to look at the Power Arch Build Tools reference manual and the manual with Targeting in the title. (The manual names very somewhat between CW distributions, but Targeting is the consistent term used in all of them.) These will give the information you need--particuarly the Targeting manual--on how to build a program. Also check out the Quick Start document, located in the CodeWarrior folder.

For exhaustive reference information on the PowerPC architecture, along with downloadable docs, check out this link.

I've attached a PowerPC Family: A Programmer's Reference Guide which might not be the exact title you're looking for, but it has a basic summary of the registers and instruction set.

---Tom


Message Edited by J2MEJediMaster on 2007-09-18 11:51 AM
0 Kudos
Reply