CWTAP_GDB_P1010_P4080 (P1010 and P4080 XML and Initialization for GDB debugging)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CWTAP_GDB_P1010_P4080 (P1010 and P4080 XML and Initialization for GDB debugging)

1,415 Views
melbournebob
Contributor I

I'm using the P1010RDB along with a CodeWarrior TAP and  Power Architecture TIP.

I'm having a little trouble understanding the settings for the TLB1 entries.

I downloaded the CW_TAP_GDB_P1010_P4080 (filename gdb_test_ccs_365.tar.gz), I found the only documentation explaining the three longwords (96 bits) displayed for a TLB1 table entry are in the comments as follows in the bin/p1010_init.gdb file:

    #                                            0            20   21        29             39        40        41

    # data format of l2mmu_cam = EPN(20)::TS::TID(8)::MASK(10)::IPROT::VALID::IPROT_dup::

    #                                            RPN(24)::UR::UW::UX::SR::SW::SX::X(2)::WIMGE(5)::U(4)::TSIZE(4)::SHEN::IPROT::spare

    #                                            42           66   67   68    69   70   71   72     74             79     83            87       88        89

 

After the comment above the p1010_init.gdb file sets the TLB1 entrys:

   echo Set TLBs\n

   set $mmu_l2_tlb1_2={0xE0000000, 0x1FC38000, 0x07140A80}

   set $mmu_l2_tlb1_3={0xFE000000, 0x7FC3F800, 0x07140E80}

   set $mmu_l2_tlb1_4={0xFF000000, 0x7FC3FC00, 0x07140E80}

   set $mmu_l2_tlb1_5={0x80000003, 0xFFC20000, 0x07141480}

   set $mmu_l2_tlb1_6={0xEFC00000, 0x0FC3BF00, 0x07140880}

   set $mmu_l2_tlb1_7={0xEFB00000, 0x0FC3BEC0, 0x07140880}

 

I examined the contents of the TLB before any of the modifications were written above (I placed an "info registers" before the first "set $mmu_l2_tlb1_2 ...") and it shows the following for the zero'th entry in TLB1:

   mmu_l2_tlb1_0 {0xfffff000, 0x1c3ffff, 0xc71402c0}

As I understand it this entry should be mapping the last 4 Kbytes of memory space (flash) that encompasses the reset vector (0xFFFFFFFC).

The TLB1 definition in the comments show the 'spare' field is the least significant 7 bits of the 3rd word.

Why does the default TLB1 entry 0 have a bit set in this 'spare' field?

Labels (1)
0 Kudos
Reply
3 Replies

892 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following detailed information of TLB1 register.

pastedImage_1.png

pastedImage_2.png

0 Kudos
Reply

892 Views
melbournebob
Contributor I

The internal representation of the TLB entry is interesting, but it doesn't really answer how the 3 longwords (96 bits) of the TLB entry as viewed in GDB map into the 191 bits of the internal TLB entry.

Also, I specifically was interested in why a spare field seemed to have a bit set in it by default (as viewed in GDB).

0 Kudos
Reply

892 Views
saqlain_raza
Contributor I

The internal representation of the TLB entry is interesting, but it doesn't really answer how the 3 longwords (96 bits) of the TLB entry as viewed in GDB map into the 191 bits of the internal TLB entry.

Did anyone find out how this mapping from 191 to 96 bits takes place ? I haven't been able to find any documentation regarding this transformation.

0 Kudos
Reply