CW for MobileGT V9 - Processor Expert for MPC5125 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW for MobileGT V9 - Processor Expert for MPC5125 ?

530 Views
queequeg
Contributor I

I have the latest CodeWarrior mobileGT version and it has Processor Expert (PE) for MPC5121E not MPC5125.

The MPC5125 is significantly different chip and the BGA pinout etc is much different.

MPC5121E is 516 pins and the MPC5125 is 324 pins.

I cant find any decent information on the pin multiplexing for the MPC5125 BGA.  PE is great for all that but the chip used is the MPC5121E which really doesnt help.

Is there a PE for MPC5125 ?

Is there a some kind os software or spreadsheet that groups the chips features and functions with corresponding BGA pins and if I want one feature it will effect not getting another feature because of overlapping pins etc.

The best world would be MPC5125 for PE.

I know about the MPC5125 Datasheet that calls out the pins but I would like a better way to view/organize the pins.

 

Thanks in Advance,

Queequeg

Labels (1)
0 Kudos
Reply
1 Reply

327 Views
ProcessorExpert
Senior Contributor III
This discussion was moved to a better location.
0 Kudos
Reply