CW for MPC5517 V2.3 Special edition limitation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW for MPC5517 V2.3 Special edition limitation

1,422 Views
Hossam
Contributor I
Hello All,

I am using the CW for MPC55xx V2.3 Special edition and I don't see any declared limitation on the web site except for the code size not to exceed 128 KB. Do you know any other limitation, espicially for debugging?? Please help

Thanks,
Hossam
Labels (1)
0 Kudos
1 Reply

205 Views
stanish
NXP Employee
NXP Employee
Hello Hossam,

The CW for MPC55xx v2.3 Special Edition includes 3-rd party debugger by Pemicro.
According to Pemicro debugger release notes with CodeWarrior Special Edition, the P&E software is limited for use with object code whose size is 128KB or less. 
So that should be the only limitation.
For more information about P&E debugger I'd suggest you to contact Pemicro support.

Stanish
0 Kudos