CW 10: Could not set PC to entry point.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10: Could not set PC to entry point.

1,490 Views
Anto25
Contributor I

I'm using CW v10.0 and I'm trying to run a program on a ColdFire 52259. I used "Flash File to Target" and clicked "Program with Erase" and it appears to work correctly as it doesn't throw any errors in its output.

But when I go to Debug mode and it tries to run, I get the following error:

"'Launching task_example Int Flash Debug' has encountered a problem. Could not set PC to entry point. "

 Does anyone have any idea what went wrong and how to fix this? It would be much appreciated. 

Labels (1)
0 Kudos
Reply
1 Reply

676 Views
BlackNight
NXP Employee
NXP Employee

I assume you are using OSBDM as connection?

I had that error message with an older OSBDM firmware.

You need to make sure that you are using the latest OSBDM firmware (on the board) and drivers (on the host) for MCU10.

You find the OSBDM firmware as well inside your MCU10 installation: {InstallDir}\Drivers\osbdm-JM60

 

BK

0 Kudos
Reply