CodeWarrior for QorIQ Knowledge Base

cancel
Showing results for 
Search instead for 
Did you mean: 

CodeWarrior for QorIQ Knowledge Base

Labels
  • General 28

Discussions

Sort by:
For use of CWTAP/USBTAP with CodeWarrior to connect target board, connection error is the type of issues that happened commonly.   How to deal with it? Attached are tips for some general things to check, here assuming target device is Power Architecture, and the tap is USBTAP or CWTAP/USB. For other targets it may be similar in some tips.   There might be variable reasons for the connection error, if the common tips in the attachment could not solve the problem, please enable CCS log and post on Freescale community or contact Freescale technical support for help. See attachment for steps to enable logging.   Also there are two useful documents in C:\Freescale\CW_PA_v10.4.0\PA\Help\PDF: CodeWarrior TAP User Guide.pdf and USB TAP User Guide.pdf.   Welcome any correction and supplement for the tips. Make CodeWarrior connection easier!
View full article
U-Boot Debug using CodeWarrior for QorIQ LS series – ARM V7 ISA
View full article
The advantages we can get out of QorIQ processing platforms are merged into so many applications!  Just to mention some, we can find it within networks, mobile wireless infrastructure, automated functions, medical use, and many many more! This way you can get high-performance communications, base stations and computing systems to market easier with its advanced tools, multiple cores, accelerators, security and more. Some service packs have been released to empower your design in this handful technology. The forth of them is being presented here with the Power Architecture Processors v10.1.2 Service. This time, the improvements have been applied in the following devices: P4040 DS       Bare-metal support       U-boot debug P4080 DS       Bare-metal support       U-boot debug P3041 DS Hydra       Linux Kernel and Application Debug P3041 DS SuperHydra       Linux Kernel and Application Debug   There are many more new features added and improved for Power Architecture Processors v10.1.2 Get to meet them in the Release Note! And download now the Service Pack 4 for Linux !   You rather Windows version ?
View full article
Good news everyone!   CodeWarrior for Power Architecture has now been updated! This wonderful combination is designed to bring out the full potential of your communication and networking applications. The CodeWarrior IDE integrated within the Eclipse development framework, combines Linux® build tools and highly advanced multiprocessor, along with multicore debugging with software analysis capabilities, allowing you to build, debug and optimize the performance of Freescale Power Architecture-based multicore applications.   What's NEW in it? Updated Documentation New IDE features (based on Eclipse Indigo 3.7.1, click here to know more!) New Debugger Features (specific to Power Architecture devices) New processor support Regular FEATURES Eclipse IDE Flash programmer Hardware diagnostics Linux application debug Bare-Board multicore debug (restrictions based on suite) Integrated GCC Build Tools/Project Management Linux Trace (Linux Based Software) Linux Kernel Debug (restrictions based on suite) CodeWarrior Build Tools (restrictions based on suite) Trace (bare metal; selected cores only) (restrictions based on suite) Performance analysis (selected cores only) (restrictions based on suite) Works with CodeWarrior TAP, Gigabit TAP and USB TAP control probes   If you wanna know more about it, take a look at the Release Note or go to the Freescale web page. If you want to star with the download at once, click here!  
View full article
Mentor Graphics makes available to the public (licensed, but free of charge) their Embedded Performance Library (MEPL) that adds Altivec support to projects built using e6500 gcc tools (version 4.7.2 or later.)  This file explains how to add that support to a CodeWarrior PA10.3.3 project for T4240QDS.
View full article