You'll need this Tips for your brand new CodeWarrior TAP! (Power Architecture)

cancel
Showing results for 
Search instead for 
Did you mean: 

You'll need this Tips for your brand new CodeWarrior TAP! (Power Architecture)

No ratings

You'll need this Tips for your brand new CodeWarrior TAP! (Power Architecture)

Freescale CodeWarrior Tap Tip

There's a ton of devices that can be debugged out with the new TAP kit for CodeWarrior. If you already met this TAP, today I'd like to introduce the CWH-CTP-COP-YE which is a removable probe tip targeted for Power Architecture processors, meant to connect the Power Architecture microprocessor target system’s JTAG port to the CodeWarrior TAP base unit’s 30-pin target connector.

 

This tip is totally compatible with the CodeWarrior TAP that I've been talking about (CWH-CTP-BASE-HE) base unit, and if you are intending to use it on Power Architecture-supported devices, you'll need to get one of these Tips specially built for the occasion. Check out some of its features up next!

 

Features

  • Removable probe tip
  • Low cost and economical to order several spares
  • Allows base unit to work with several different target types

 

System Requirements

 

Labels (1)
Version history
Revision #:
1 of 1
Last update:
‎09-21-2012 04:41 PM
Updated by: