#ifndef __MENU_H__#define __MENU_H__#include "PE_Types.h"#include "PE_Error.h"//定义菜单项数据结构typedef struct menu1{ byte MenuType; //本菜单种类 byte MenuName[15]; //本菜单名称 byte MenuFunctionInfo[30]; //本菜单功能说明 byte *pMenuLeftInfo; //本菜单Left键功能说明 byte *pMenuRightInfo; //本菜单Right键功能说明 const struct menu1 *pFarther; //定义父菜单指针 const struct menu1 *pSon; //定义子菜单指针 const struct menu1 *pPre; //定义上一个兄弟菜单 const struct menu1 *pNext; //定义下一个兄弟菜单 void (*far pOn_OK_Button)(void); //OK键处理函数指针 void (*far pOn_Left_Button)(void); //Left键处理函数指针 void (*far pOn_Right_Button)(void); //Right键处理函数指针}Menu_t;void Menu_On_OK(void);void Menu_Go_Pre(void);void Menu_Go_Next(void);void Menu_Config_On_OK(void);void Menu_Run_On_OK(void);#endif
#ifndef __SETTINGSCREEN_H__#define __SETTINGSCREEN_H__#include "PE_Types.h"#include "Menu.h"#include "MenuRes.h"#include "stddef.h"void SettingScreen(byte keyBuf); //画面结构显示函数#endif
#include "Menu.h"#include "MenuRes.h"#include "SettingScreen.h"#include "LQ12864.h"#include "stddef.h"#include "PE_Types.h"#include "Events.h" /*当前菜单指针*/Menu_t const *pCurrentMenu, *pCurrntmenuPre, *pCurrentMenuNext, *pCurrentMenuNextNext; //当前菜单组指针Menu_t const (*pCurrentMenuList)[]; /*---current menu pointer init to first level menu---*/pCurrentMenu = MenuList_Top; //err here not decl /*---current menu arry pointer init to first level menu arry---*/pCurrentMenuList = MenuList_Top;void SettingScreen(byte KeyBuf){ byte i, Menu_item_num, Menu_item_disp_num; byte Jiantou = 66; byte *pJiantou = &Jiantou; //get the number of current menu arry Menu_item_num = sizeof(*pCurrentMenuList) / sizeof(Menu_t); //get the number how many items to display on screen //if less than 4 , display all, otherwise display 4 if(Menu_item_num < 4) Menu_item_disp_num = Menu_item_num; else Menu_item_disp_num = 4; //display crrent menu's left key function info LCD_CLS_XY(2, 0, 128, 0); LCD_P6x8Str(2, 0, pCurrenMenu->pMenuLeftInfo); //display crrent menu's right key function info LCD_CLS_XY(2, 1, 128, 1) LCD_P6x8Str(2, 1, pCurrentMenu->pMenuRightInfo); //display crrent menu's function info LCD_CLS_XY(2, 6, 128, 7); LCD_P6x8Str(2, 6, pCurrentMenu->MenuFunctionInfo); //display fouce menu sign arry LCD_P6x8Str(12, 3, pJiantou); //to display menus in crrent menulist if(Menu_item_disp_num > 1) // if menu items more than one { //first menu item pCurrentMenuPre = pCurrentMenu->pPre; LCD_CLS_XY(20, 2, 100, 2); LCD_P6x8Str(20, 2, pCurrennMenuPre->MenuName); } if(Menu_item_disp_num > 0) //we always get menu to display { LCD_CLS_XY(20, 3, 100, 3); LCD_P6x8Str(20, 3, pCurrentMenu->MenuName); } if(Menu_item_disp_num > 2) { pCurrentMenuNext = pCurrentMenu->pNext; LCD_CLS_XY(20, 4, 100, 4); LCD_P6x8Str(20, 4, pCurrentmenuNext->MenuName); } if(Menu_item_num > 3) { pCurrentMenuNextNext = pCurrentMenuNext->pNext; LCD_CLS_XY(20, 5, 100, 5) LCD_P6x8Str(20, 5, pCurrentMenuNextNext->MenuName); } switch(KeyBuf) { case Button_OK: if(pCurrentMenu->pOn_OK_Button != NULL && pCurrentMenu->pSon == NULL) { *pCurrentMenu->pOn_OK_Button(); } else { if(pCurrentMenu->MenuName == "Done") { pCurrentMenu = pCurrentMenu->pFarther; } else { pCurrentMenu = pCurrentMenu->pSon; } } break; case Button_Left: if(pCurrentMenu->pPre == NULL && pCurrentMenu->pNext == NULL && pCurrentMenu->pOn_Left_Button != NULL) { *pCurrentMenu->pOn_Left_Button(); } else { pCurrentMenu = pCurrentMenu->pPre; } break; case Button_Right: if(pCurrentMenu->pNext == NULL && pCurrentMenu->pPre == NULL && pCurrentMenu-pOn_Right_Button != NULL) { *pCurrentMenu->pOn_Right_Button(); } else { pCurrentMenu = pCurrentMenu->pNext; } break; default: break; }}
NAMESENDSEGMENTS /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */ RAM = READ_WRITE 0x2000 TO 0x3FFF; ROM_4000 = READ_ONLY 0x4000 TO 0x7FFF; ROM_C000 = READ_ONLY 0xC000 TO 0xFEFF; PAGE_F8 = READ_ONLY 0xF88000 TO 0xF8BFFF; PAGE_F9 = READ_ONLY 0xF98000 TO 0xF9BFFF; PAGE_FA = READ_ONLY 0xFA8000 TO 0xFABFFF; PAGE_FB = READ_ONLY 0xFB8000 TO 0xFBBFFF; PAGE_FC = READ_ONLY 0xFC8000 TO 0xFCBFFF; PAGE_FE = READ_ONLY 0xFE8000 TO 0xFEBFFF;ENDPLACEMENT /* here all predefined and user segments are placed into the SEGMENTS defined above. */ _PRESTART, /* Used in HIWARE format: jump to _Startup at the code start */ STARTUP, /* startup data structures */ ROM_VAR, /* constant variables */ STRINGS, /* string literals */ NON_BANKED, /* runtime routines which must not be banked */ COPY INTO ROM_C000, ROM_4000; DEFAULT_ROM INTO PAGE_FE, PAGE_FC, PAGE_FB, PAGE_FA, PAGE_F9, PAGE_F8; DEFAULT_RAM /* all variables, the default RAM location */ INTO RAM;ENDINIT _EntryPoint /* The entry point of the application. This function is generated into the CPU module. */STACKSIZE 0x0080 /* Size of the system stack. Value can be changed on the "Build options" tab */
err message in attched picture
解決済! 解決策の投稿を見る。
Menu_t const *pCurrentMenu, *pCurrntmenuPre, *pCurrentMenuNext, *pCurrentMenuNextNext;
pCurrentMenu = MenuList_Top; // <--- this can't be done outside the function body
------------------------
But you can initialize your variable this way:
Menu_t const *pCurrentMenu = MenuList_Top, *pCurrntmenuPre, *pCurrentMenuNext, *pCurrentMenuNextNext;
Menu_t const *pCurrentMenu, *pCurrntmenuPre, *pCurrentMenuNext, *pCurrentMenuNextNext;
pCurrentMenu = MenuList_Top; // <--- this can't be done outside the function body
------------------------
But you can initialize your variable this way:
Menu_t const *pCurrentMenu = MenuList_Top, *pCurrntmenuPre, *pCurrentMenuNext, *pCurrentMenuNextNext;
Thanks, the probem solved.
sorry for posted wrong place