why my codewarrior HCS08 5.1 create a new project will close the codewarrior window?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

why my codewarrior HCS08 5.1 create a new project will close the codewarrior window?

跳至解决方案
1,975 次查看
KingZhang
Contributor I
why my codewarrior HCS08 5.1  create a new project or click open project button ,will close the codewarrior window?but no this problem on my notebook .
 
I think the codewarrior if ready to using "open folder" or "create file or folder" window ,this problem will appear.
 
my computer operating system is Windows XP SP2.
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
984 次查看
CompilerGuru
NXP Employee
NXP Employee
High KingZhang,

there has been a reported incompatibility with MS Office 2007 with these symptoms in this forum.
See this thread for the case, it also contains a workaround.

http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=3747&query.id=4082#M3...


Daniel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
985 次查看
CompilerGuru
NXP Employee
NXP Employee
High KingZhang,

there has been a reported incompatibility with MS Office 2007 with these symptoms in this forum.
See this thread for the case, it also contains a workaround.

http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=3747&query.id=4082#M3...


Daniel
0 项奖励
回复
984 次查看
KingZhang
Contributor I
Hi,CompilerGuru
 
I'm Uncheck "Run this program in compatibility mode for". it works beautifully.
 
Thanks your help,
 

 
0 项奖励
回复