what is the pinout for header connector on codewarrior tap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the pinout for header connector on codewarrior tap

943件の閲覧回数
martysmith
Contributor I

I am looking for the signal pinout of the codewarrior tap so that I can interface coldfire v2 core which is installed on a board developed by Arturus Networks which is not the standard 26 pin BDM interface. Arcturus has provided the 18 pin connector pin out for their board but I don't know the signals on the Codewarrior Tap module. If it matters I have the Rev E one.

ラベル(1)
0 件の賞賛
返信
1 返信

838件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Marty,

You can find the ColdFire 26-pin BDM connector information in the chapter 7 on the following document:

http://cache.nxp.com/files/soft_dev_tools/doc/user_guide/UTAPUG.pdf 

pastedImage_2.png


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信