the CW10.6 command line tools question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the CW10.6 command line tools question

Jump to solution
1,132 Views
wangpeng
Contributor I

Hi:

I link a project used the command line tools ,and  the commands is copy from CW10.6 setting ,but the tools had an err "undefined: '__start'",when i run the command .I can find the file"__start.c",but I do not know how to define the __start?

Labels (1)
0 Kudos
Reply
1 Solution
976 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello peng

Please check the settings for the access path has been configured correctly, it should contains the path for the head file which includes the external function declaration for '__start '.

For details, please refer to the compiler manual for your MCU.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
977 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello peng

Please check the settings for the access path has been configured correctly, it should contains the path for the head file which includes the external function declaration for '__start '.

For details, please refer to the compiler manual for your MCU.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
976 Views
wangpeng
Contributor I

Hi:

I had check the settings, and add the path of the "__start.c",and the header files , but it had a Undefine "__start" err also.and can you provide some examples about the command line tools for mpc56xx to me? or the example about CW API .

i can found several datasgeet about the commandline tools.

thank you!

2016-05-06

王鹏

控制部

北京亿华通科技股份有限公司

地址:北京市海淀区永丰产业基地永澄北路绿海大厦A座4层

邮编:100094

电话:+86 10 56382035/36/37/38-120

传真:+86 10 56382035-162

手机:13167398738

网址:http://www.sinohytec.com

邮箱:wangpeng@autoht.com

发件人:TICS_Fiona <admin@community.freescale.com>

发送时间:2016-05-04 15:34

主题:Re: - the CW10.6 command line tools question

收件人:"peng wang"<wangpeng@autoht.com>

抄送:

NXP Community

the CW10.6 command line tools question

reply from Xin Kuang in CodeWarrior for MCU - View the full discussion

Hello peng

Please check the settings for the access path has been configured correctly, it should contains the path for the head file which includes the external function declaration for '__start '.

For details, please refer to the compiler manual for your MCU.

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 Kudos
Reply