target request failed failed to set breakpoint

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

target request failed failed to set breakpoint

575 次查看
Mockingbird
Contributor I

I am running Codewarrior for MCU version 11.0.1 build 180609 with an MC9S08GT16a.  My project is a relocatable assembly project.  When I try to run the debugger, I get a pop-up saying "Error stopping at main.  Reason: Target request failed: Failed to set breakpoint.  Continue?"  If I click "Yes" the debugger starts and seems to run normally.  But what is the source of the annoying pop-up?

Previous threads on this problem have been no help.  When I created a new project with the same source files, I got the same pop-up.  And the "Strip symbolic information" box is not checked.

0 项奖励
1 回复

389 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Timothy Phillips 

Is there any problem if you test your code in full chip simulation mode?

Is this problem in any relocatable assembly code?

if this is not a common issue, please upload your demo project, we can check it directly.

Best Regards

Jun Zhang

0 项奖励