software notification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

software notification

跳至解决方案
2,246 次查看
Mei
Contributor IV

Can you help me please.  I have an easy question. I got the following software notification

-------------------------------------------------------------------------

software notification

Hello,

Thank you for your interest in CWX-MCU-PROED-EX_11-1. We hope you are enjoying your experience developing with NXP software.

Our records indicate that your product will expire on 03/19/2019.

As always, please feel free to contact us with any questions you may have at nxp.com/support.

Thank you for including NXP as part of your solution.

----------------------------------------------------------------------

I tried to answer in several ways, but that was probably not intended.

my text therefore here.

------------------------------------------------------------------------

Thank you for your reminder.

I have download this CodeWarrior f. MCU v.11.1. and want to use it to program an 8.bit nxp controller.

I still need to do something to use this software. I have not started it yet because I do not have a development board yet.

--------------------------------------------------------

What should I do? Do I have to register the software and how? 

Gerd Meinert

1 解答
2,023 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Gerd Meinert,

Thanks for contacting our technical support, I will serve for you.

There are four CW licenses: Special, Basic, Standard, Professional. About detail please refer to

CW suites quick reference guide, I attach if for you.

When just download and install, by default, it can used as Professional version in 45 days, after that,

it will change to Special version.

If the Special version can meets your requirement, you needn't to anything, just ignore that information.

If can't . you can refer to your needs to buy CW license.

This is for Special editions:

pastedImage_2.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,024 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Gerd Meinert,

Thanks for contacting our technical support, I will serve for you.

There are four CW licenses: Special, Basic, Standard, Professional. About detail please refer to

CW suites quick reference guide, I attach if for you.

When just download and install, by default, it can used as Professional version in 45 days, after that,

it will change to Special version.

If the Special version can meets your requirement, you needn't to anything, just ignore that information.

If can't . you can refer to your needs to buy CW license.

This is for Special editions:

pastedImage_2.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,023 次查看
Mei
Contributor IV

Hello

Now I underständig software notification.

It is a friendly reference to this context.
Thank you

0 项奖励
回复