remove file properties

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

remove file properties

1,219 次查看
asmith
Contributor III

How do I remove properties (such as optimization settings) set for a specific file so that it reverts back to using those for the folder or project ?

标签 (1)
0 项奖励
回复
2 回复数

1,102 次查看
trytohelp
NXP Employee
NXP Employee

Hi David,

The configuration can be linked to the project (all files included), folder or specific to a file.

If the properties is opened when the project is selected you will open the Project Properties.

If the properties is opened when a file is selected, you will open the file properties.

The File properties is applied on file only whereas the project properties is applied on all files included in the project.

If you open the file properties and click on "Restore Defaults" the options defined in the project properties will be applied.

If you've a specific Folder properties (different to project) when "Restore Defaults" is applied on file the options defined in the project are used.

Hope this will answer your question


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,102 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello David,

Do you use CodeWarrior ? Which version ? And about which chip ?

BR

Alice

0 项奖励
回复