"An internal error occurred during: "Setting up indexer". (CW 10.6)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"An internal error occurred during: "Setting up indexer". (CW 10.6)

1,586件の閲覧回数
flacca
Contributor II

I get the following error at startup (CW 10.6): "An internal error occurred during: "Setting up indexer". As a result the indexer isn't functioning. Can any provide assistance on resolving this?

ラベル(1)
0 件の賞賛
返信
1 返信

1,314件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

first I suggest you remove .metadata folder in your current workspace or create a new workspace to check if it can fix the problem.

If the problem still exists, please refer Erich's article.

https://mcuoneclipse.com/2012/03/20/fixing-the-eclipse-index/

if still can not fix the problem, please use the latest CW10.7 which fixes many bugs of 10.6.

CodeWarrior for MCU V10.7 is available for download from nxp.com (http://www.nxp.com/cwmcu10).

See https://community.nxp.com/docs/DOC-332444 and release notes (attached) for additional details.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信