problems with CW05

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

problems with CW05

跳至解决方案
2,155 次查看
teruko
Contributor I
Hello,
I'd like to use the project EVK_Switch_Demo (this project is  included in BeeKit Wireless Connectivity Toolkit Rev. 0.0 - 10/2006)  with CW v5.0 for HC(s)08, but when I link, I have the follow message:
Link Error : L1936: ELF output: Burner Error: Could not open the Link
Burner output file.

Link Error : Link failed
Please, what can I do to run this ready project ( there is a  message that this project was created with CW v3.1)??
Thank you!!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,255 次查看
trytohelp
NXP Employee
NXP Employee
This problem has been logged in the Freescale data base under the 1-342881601.
This issue will be investiagte by the support team.
 
Pascal

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,256 次查看
trytohelp
NXP Employee
NXP Employee
This problem has been logged in the Freescale data base under the 1-342881601.
This issue will be investiagte by the support team.
 
Pascal
0 项奖励
回复