please i need to advice for 9s08 instruction about   DIV

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

please i need to advice for 9s08 instruction about   DIV

Jump to solution
2,500 Views
kiwonlee
Contributor I

seen to instruction  DIV is 16bit divide by 8bit division instruction. but result is store to 8bit ACCA only.

how can i using this instruction when real 16/8?

Labels (1)
0 Kudos
Reply
1 Solution
2,356 Views
Rick_Li
NXP Employee
NXP Employee

Hi Ki Won Lee,

May be the below code could help you!

int x;

char y;

char z;

void main(void) {

...

  x= 300;

  y = 25;

  __asm {

      ldhx x;

      lda y;

      div

  }

...

}

View solution in original post

0 Kudos
Reply
6 Replies
2,356 Views
Leojunin
Contributor IV

Hi. the instruction works like this: H:A / X. Must load the 16-bit value (dividend) in H:A as a single record and the divisor in X.

You can use the following:

Load H:X with LDHX instruction and pass the value of X to A. Then load X with the divider 8 bits.

Example:

          LDHX #4532

          TXA

          LDX  #34

          DIV

The cocient in ACCA the remainder in H. thus, leading to 0 in A is a decimal add to divide again

Ej2. another way:

          LDA  #45

          PSHA

          PULH

          LDA  #32

          LDX  #34

          DIV

EDiting: I saw a response HX / A. It's wrong. It's not how it works.

0 Kudos
Reply
2,356 Views
kiwonlee
Contributor I

thanks, yong li,Edward

just catching usage of 8bit DIV instruction.

help from Edward's explanation.

0 Kudos
Reply
2,357 Views
Rick_Li
NXP Employee
NXP Employee

Hi Ki Won Lee,

May be the below code could help you!

int x;

char y;

char z;

void main(void) {

...

  x= 300;

  y = 25;

  __asm {

      ldhx x;

      lda y;

      div

  }

...

}

0 Kudos
Reply
2,356 Views
kiwonlee
Contributor I

thanks Yong li  interest my question. 

i would give you ask one more time.

in your example code set  x = 300 and y = 25  maybe get good result 12 in acca . what about y = 1?

acca result is 5?.....  i don't understand this instruction..

0 Kudos
Reply
2,356 Views
kef2
Senior Contributor V

It is very similar to how kids divide 2-digits numbers by 1-digit number on paper. They divide first digit, and then (one only) digit remainder * 10 + next digit. Difference is that we have now bytes instead of decimal digits, rules of math are the same.

unsigned short num= 300;

unsigned char  denom = 25;

unsigned short quotient;

unsigned char remainder;

//DIV instruction   H:A / X = A, rem H

  __asm {

      ldx denom

      clrh

      lda num:0; // first digit

      div

      sta quotient:0

      lda num:1 // next digit

      div

      sta quotient:1

      pshh

     pula

     sta  remainder

  }

0 Kudos
Reply
2,356 Views
kiwonlee
Contributor I

thanks Edward.

then when i using index register high  H ?

0 Kudos
Reply