pe micro usb multilink can't connect to codewarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pe micro usb multilink can't connect to codewarrior

1,641 Views
xiangxu860
Contributor II

recently I got a new computer and setup the codewarrior  V10.7  .

I met a problem when I debugged the project.  My pe micro usb multilink  can't  connect to codewarrior.

1.png

then I  press the 'refresh ' button ,error dialog box come out .

2.png

3.png

how can I fix it ?

ps.  My pe micro usb multilink  can work well with another computer .

0 Kudos
Reply
1 Reply

1,508 Views
xiangxu860
Contributor II

I have fixed this problem.

The default driver of PE-micro may have some errors. I delete it from Device Manager as shown below.

QQ图片20170706080944.jpg

Then I connect the PE-micro  to my computer  ,and it works well .

0 Kudos
Reply