Hello,
I’m using the HCS12 TB with the mc9s12dp512 chip and I want to use the msCAN feature on the chip.
Does anyone has an example how to initialize CAN0 to send and receive messages from and to another HCS12 TB.
It would be great if there was also an example how I can send and receive a massage. I want to use the receive interrupt to read a message.
I’ve a code but it isn’t working and I don’t understand the msCAN feature completely.
I’m testing it with the loop back option in the CAN0CTL1 register. And when this is working I want to test it between 2 MCU’s. Eventually I want to communicate between 3 HCS12 T-Boards.
Thanks in advance.
Greetings dan23
Hello,
I’ve already 3 HCS12 T-boards with the mc9s12Dp512 chip in my possession. So switching to another chip isn’t an option.
msCAN is working now on 1 board when I use the loop back mode.
It isn’t working when I want to communicate between 2 HCS12 boards. Is it a wrong initialization for CAN0?
void SetCan0(void)
{
CAN0CTL1_CANE = 1; //enable CAN, required after reset
//----------------------------------------------------------------
CAN0CTL0_INITRQ = 1; //MSCAN in Initialization Mode.
while(!CAN0CTL1_INITAK); //The registers CANCTL1, CANBTR0, CANBTR1,
//CANIDAC, CANIDAR0-7, CANIDMR0-7 can
//only be written by the CPU when the MSCAN
//is in Initialization Mode.
//----------------------------------------------------------------
//Initialization Mode
CAN0CTL1 = 0xC0; //The MSCAN module is enabled.
//The MSCAN clock source is the Bus Clock.
//Loop Back Self Test disabled with 0xC0 and
//enabled with 0xE0
CAN0BTR0 = 0x08; //SJW 1 Tq clock cycles
//Prescaler value (8)
CAN0BTR1 = 0x14; //One sample per bit.
//Time Segment 2 = 2 Tq clock cycle
//Time Segment 1 = 5 Tq clock cycle
//For standard identifiers, only the first two (CANIDAR0/1,
//CANIDMR0/1) are applied
CAN0IDMR0 = 0b00000000;
CAN0IDMR1 = 0b00011111;
CAN0IDAR0 = 0b00100010;
CAN0IDAR1 = 0b00000000;
CAN0IDAC = 0x10; //Four 16 bit Acceptance Filters
//----------------------------------------------------------------
CAN0CTL0_INITRQ = 0; //MSCAN in Normal operation.
while(CAN0CTL1_INITAK); //following reg can only be written by the
//CPU when the MSCAN out of Initialization
//Mode.
//----------------------------------------------------------------
//Normal operation.
CAN0CTL0 = 0x00; //The module is not affected during Wait Mode.
//Disable internal MSCAN timer.
//Wake-Up disabled The MSCAN ignores traffic on CAN.
//Running The MSCAN functions normally.
CAN0RIER = 0x01; //A receive buffer full (successful message
//reception) event causes a receiver interrupt
//request.
CAN0TBSEL = 0x01; //TX0 message Buffer is selected, if lowest
//numbered bit.
}
greetings dan23
reg_CANCTL1(port) = CANE; /* can enable (write once), no special modes */ /* Note! CANE must be set before sleep mode can be entered */ reg_CANCTL0(port) |= SLPRQ; /* sleep mode */ reg_CANCTL0(port) |= INITRQ; /* init mode */ { while((reg_CANCTL1(port) & SLPAK)==0) /* wait until CPU enters sleep mode. */ { ; } reg_CANCTL1(port) |= CLKSRC; /* clksrc=bus */ *(uint16*)®_CANBTR0(port) = baudrate; if(filter != NULL) { if(filter->type == BASIC_CAN) { reg_CANIDAC(port) = 0x10; /* 4 x 16-bit filters */ } else /* type == EXTENDED_CAN */ { reg_CANIDAC(port) = 0x00; /* 2 x 32-bit filters */ } *(uint32*)®_CANIDAR0(port) = filter->id_accept._32bit[0]; *(uint32*)®_CANIDAR4(port) = filter->id_accept._32bit[1]; *(uint32*)®_CANIDMR0(port) = filter->id_mask._32bit[0]; *(uint32*)®_CANIDMR4(port) = filter->id_mask._32bit[1]; } /* if(filter != NULL) */ } reg_CANCTL0(port) &= ~SLPRQ; /* leave sleep mode */ reg_CANCTL0(port) &= ~INITRQ; /* leave init mode */ if(useRxInterrupt) { reg_CANRIER(port) = RXFIE; } while ((reg_CANCTL1(port) & (SLPAK|INITAK)) > 0) /* wait until CAN is running */ { ; }