I am running Code Warrior V5 for 9S12 with a P&E USB BDM Multilink.
I have no problem erasing and programming PFLASH (program flash), but I have not been able to erase or program DFLASH (data flash).
Here is what I did and the responses I got:
in>flash init autoid
FP: FLASH parameters loaded for MC9S12XEQ384_V3(NVMIF2 rev 1,1,1,1,1) from C:\Freescale\CodeWarrior_for_S12X_V5_0\prog\FPP\mcu02DB.fpp
MCU clock speed: 4017000 Hz
Block Module Name Address Range Status
0 PFLASH 4000 - 7FFF Blank - Unselected
1 PFLASH C000 - FFFF Blank - Unselected
2 PFLASH E08000 -E7BFFF Blank - Unselected
3 PFLASH F08000 -FFBFFF Blank - Unselected
4 DFLASH 800 -1F0BFF Programmed - Unselected
in>flash erase 4
Vppon command file is disabled.
Vppoff command file is disabled.
in>flash
MCU clock speed: 4017000 Hz
Block Module Name Address Range Status
0 PFLASH 4000 - 7FFF Blank - Unselected
1 PFLASH C000 - FFFF Blank - Unselected
2 PFLASH E08000 -E7BFFF Blank - Unselected
3 PFLASH F08000 -FFBFFF Blank - Unselected
4 DFLASH 800 -1F0BFF Programmed - Unselected
in>
I also tried using "flash select 4" before erasing, but the result was no different.
解決済! 解決策の投稿を見る。
S12XE doesn't have dedicated commands to erase only D-FLASH. Erase All Blocks and Unsecure command (0xB) contrary to reference manual don't erase D-FLASH. Now, since partitioning commands are missing in debugger, the only solution I see is issuing partitioning commands from user code.
To fully erase and repartition D-FLASH, one may need to execute Full Partition D-Flash command. This command works only in special modes. So code may need to check if operating in special single chip mode under debugger control:
if ((MODE & 0xE0) == 0) // is it special
{
FSTAT = FSTAT_ACCERR_MASK | FSTAT_FPVIOL_MASK;
FCCOBIX = 0;
FCCOB = 0x0F00; // full partition d-flash
FCCOBIX++;
FCCOB = xxx; //DFPART
FCCOBIX++;
FCCOB = yyy; //ERPART
FSTAT &= FSTAT_CCIF_MASK;
while(!(FSTAT & FSTAT_CCIF_MASK))
{
}
}
Is D-FLASH partitioned? I'm using emulated EEPROM (EEE) and I noticed that debugger doesn't erase it. Moreover, data in EEE survives chip securing and unsecurig. I didn't try if it is the same with D-partition or in case D-flash is never partitioned. Maskset is 5M48H.
Debugger unsecure command is working well. What's weird is that unsecure cmd file is using command 8 - Erase All Blocks. S12XE RM states that "The Erase All Blocks operation will erase the entire P-Flash and D-Flash memory space including the EEE nonvolatile information register." It looks like it is not true. After this command D-FLASH is still partitioned and contents of EEE is unchanged. EEPROM Emulation Query command returns unchanged partitioning parameters.
Are you trying to load some constants along with code to D-FLASH? If so, then what addresses are you using? D-FLASH on S12XEP100, while not partitioned, is from 0x100000'G to 0x107FFF'G . This corresponds to EEPROM segments EEPROM_00 to EEPROM_1F in default prm file.
The dflash is partioned. I want to completely erase dflash so it can be repartitioned.
In the debugger, I have tried every variation of the erase command I could think of, but any but "flash erase" and "flash erase 4" (or whatever number) were rejected.
Not can I find any other commands that seem useful for this purpose.
What am I missing?
S12XE doesn't have dedicated commands to erase only D-FLASH. Erase All Blocks and Unsecure command (0xB) contrary to reference manual don't erase D-FLASH. Now, since partitioning commands are missing in debugger, the only solution I see is issuing partitioning commands from user code.
To fully erase and repartition D-FLASH, one may need to execute Full Partition D-Flash command. This command works only in special modes. So code may need to check if operating in special single chip mode under debugger control:
if ((MODE & 0xE0) == 0) // is it special
{
FSTAT = FSTAT_ACCERR_MASK | FSTAT_FPVIOL_MASK;
FCCOBIX = 0;
FCCOB = 0x0F00; // full partition d-flash
FCCOBIX++;
FCCOB = xxx; //DFPART
FCCOBIX++;
FCCOB = yyy; //ERPART
FSTAT &= FSTAT_CCIF_MASK;
while(!(FSTAT & FSTAT_CCIF_MASK))
{
}
}
Thanks.