i use 9s12xep100 . in DFLASH area i defined a const variable, but in S19 file, there is no record about this const variable.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i use 9s12xep100 . in DFLASH area i defined a const variable, but in S19 file, there is no record about this const variable.

1,071件の閲覧回数
jeffzxg
Contributor I

hi !

i use 9s12xep100 . in DFLASH area i defined a const variable,  but in S19 file,  there is no record about this const variable.

prm file like this

SEGMENTS

      EEPROM_00     = READ_ONLY   DATA_FAR IBCC_FAR  0x000800 TO 0x000BFF;
      EEPROM_01     = READ_ONLY   DATA_FAR IBCC_FAR  0x010800 TO 0x010BFF;
      EEPROM_02     = READ_ONLY   DATA_FAR IBCC_FAR  0x020800 TO 0x020BFF;

END

PLACEMENT

 CALI_DATA        INTO EEPROM_01;

END

main file like this

#pragma  DATA_SEG  __GPAGE_SEG  CALI_DATA

volatile const  unsigned int   test[3] = {1 , 3 , 4};

#pragma  DATA_SEG  DEFAULT
 

void main(void) {
  /* put your own code here */
 
  unsigned int  a_test = test[0];
  unsigned char cnt;
 
  for(cnt=0;cnt<3;cnt++)
  {
    a_test = test[cnt];
    a_test++;
  }
    
 
  for(;;)
   {
      a_test++;
   
  }
}

i use codewarrior compile this project ,  and in MAP file i checked that

- VARIABLES:
     test                                     10800       6       6       4   CALI_DATA  

bus the s19 file has no record about "test" variable


S123C000CF2100C6055B134A802CFE4A8000FE0000C015C051000000000000000000000051
S123C0200000000000000000000000000000000000000000000000000000000000000000FC
S116C04000000000000000000000000000000000000000E9
S105FFFEC0003D
S224FE8000C6105B1018FC040069ADE6808759180B100010B74518ECE204006C811862816235
S224FE802080E680C10325E318628120FBFEC011FDC00F270E35ED31EC3169700434FB3103F5
S219FE804026F2FEC013EC31270BED31180A30700434F920F10AC4
S9030000FC

my question is:   why there is no record information about DFLASH const variable "test" in s19 file.1

thanks all!

ラベル(1)
0 件の賞賛
返信
1 返信

864件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello

No EEPROM content shown in S19 file is because the burner.bbl missed non-banked EEPROM. I did the modification in burner.bbl for you, see attached.

/* logical non banked EEPROM at $0C00 to logical */
len = 0x400
origin = 0x000C00
destination = 0x000C00
SENDBYTE 1 "%ABS_FILE%"

/* logical non banked EEPROM at $0800 to logical */
len = 0x100
origin = 0x000800
destination = 0x000800
SENDBYTE 1 "%ABS_FILE%"

/* logical non banked EEPROM at $0C00 to global */
len = 0x400
destination = 0x13FC00
origin = 0x000C00
SENDBYTE 1 "%ABS_FILE%"

/* logical non banked EEPROM at $0800 to global */
len = 0x100
destination = 0x100000
origin = 0x000800
SENDBYTE 1 "%ABS_FILE%"

With the new bbl file, compile the C sample code, you can see this line added in s19 file:

S11208001245486F772061726520796F7521006A

I will also attach my demo project.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信