how to import project from classic ide 8.3 to eclipse ide 10.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to import project from classic ide 8.3 to eclipse ide 10.5

1,296 次查看
pradeepkumar
Contributor II

Any body please me know how to import project from Code Warrior Classic IDE to Code Warrior Eclipse IDE 10.5

标签 (1)
0 项奖励
回复
1 回复

1,038 次查看
TICS_Fiona
NXP Employee
NXP Employee

CodeWarrior v10.5 includes CodeWarrior Classic Project Importer for CW DSC v8.3 projects.

For how to do it, please refer to section 3.8 in CW10.5 Targeting Manual:

C:\Freescale\CW MCU v10.5\MCU\Help\PDF\Targeting_Microcontrollers.pdf

The old version of Eclipse CodeWarrior does not include Classic Project Importer, the solution is user needs to create a new bareboard project in CW10.4 and then add/copy all your source files to the new project. This is the cleanest way to import a project. CW Experts recommend to use this method rather than using the project importer. Below is an application not for how to do this:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复