headers not found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

headers not found

1,067 次查看
Jim_P
Contributor III

using the S08JM16 for a project with CW 10.1 running on Windows 7 64 bit

 

I have different directories setup in the project file.  one for the application with the code in this directory.

a different directory for the real time monitor that I have developed and use as starting code for many projects.

 

this code in in the monitor_Lib directory.  and was drag and dropped into the monitor_lib directory and option to have the code linked into the project.

 

The headers for the different files are in the Standard CW header folder.

 

the problem is that while I can select and open the header files, the compiler can not seem to find the header files.

 

any suggestion

 

thanks

Jim P

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

974 次查看
CrasyCat
Specialist III

Hello

 

Did you add the path to the include files to your project?

 

CrasyCat

0 项奖励
回复