does codewarrior work with MC9S08QD2MSC and if so, which flavor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does codewarrior work with MC9S08QD2MSC and if so, which flavor?

1,196 Views
jeffjacobson
Contributor I

I am looking for the correct IDE/compiler

0 Kudos
Reply
3 Replies

1,058 Views
jeffjacobson
Contributor I

Carlos;

Thank you for the reply. I downloaded the latest version and when I try to open a project file it says it is not supported. This is a old codewarrior project from a previous engineer who is providing no help to the company anymore. I am trying to load up the project and get it to compile. The only comment that existed was Codewarrior 5.2 was used. Any thoughts on how to get this project into the new version?

Thanks, Jeff

0 Kudos
Reply

1,058 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jeff,

The cleanest way to import the project to CodeWarrior would be to create a Bareboard project in CodeWarrior 10.7 and copy your drivers from the 5.2 project. I would recommend you to use the new linker file and startup code, just compare it with the ones in your previous project to make sure there is no need to make any changes. Also, compare the project properties to match the ones in your previous project. For detailed information please see this document:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

1,058 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jeff,

I would recommend you to use the latest CodeWarrior for MCUs version, it supports the device S08QD devices:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply