cw v2.10 OSJTAG 调试器无法使用

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cw v2.10 OSJTAG 调试器无法使用

Jump to solution
415 Views
smallyang
Contributor III

smallyang_0-1711095725028.png

 

smallyang_1-1711095755876.png

是这样的,我安装了CodeWarrior for MPC55xxMPC56xx v2.10  和CodeWarrior for MPC55XX-MPC56XX Processor Expert v2.2  然后买了一个OSJTAG下载器   现在电脑上驱动显示一个叹号   cw v2.10软件调试里面能找到flash version30.21  但是老是显示无法进入后台模式   驱动未初始化

有人遇到过这种情况吗 ,我现在特别着急,麻烦帮帮我!

Here's the thing. I installed CodeWarrior for MPC55xxMPC56xx v2.10 and CodeWarrior for MPC55XX-MPC56XX Processor Expert v2.2 and bought an OSJTAG downloader. Now the driver on the computer shows an exclamation mark. flash version30.21 can be found in the cw v2.10 software debugging, but it keeps showing that the driver cannot enter background mode and is not initialized.

Has anyone ever been in this situation? I'm in such a hurry, please help me!

 

 

 

 

0 Kudos
1 Solution
383 Views
smallyang
Contributor III

smallyang_1-1711163657161.png

 

 

请问这个是的吗?

View solution in original post

0 Kudos
3 Replies
384 Views
smallyang
Contributor III

smallyang_1-1711163657161.png

 

 

请问这个是的吗?

0 Kudos
385 Views
smallyang
Contributor III

https://community.nxp.com/t5/CodeWarrior-Development-Tools/Multilink-Universal-cannot-connect-to-MCF...

smallyang_0-1711162607994.png

 

这里有个方法下载其他版本6.83的   请问谁有这个安装包呢

0 Kudos
394 Views
smallyang
Contributor III

smallyang_0-1711156447153.jpeg

smallyang_3-1711156521491.png

 

smallyang_2-1711156494774.png

 

我在win7上也试了,驱动都能找到,但是一直进不了后台模式

I also tried on win7, the driver can be found, but has been unable to enter the background mode

 

0 Kudos