could anybody find "CW_FetalMonitor_RevX.zip " this file in freescale webpage??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

could anybody find "CW_FetalMonitor_RevX.zip " this file in freescale webpage??

994件の閲覧回数
remyarrajan
Contributor I

i have searched for  "CW_FetalMonitor_RevX.zip"  in freescale webpage but i couldn't find any.

ラベル(1)
0 件の賞賛
返信
1 返信

907件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

If I'm right you refer to the http://cache.nxp.com/files/microcontrollers/doc/ref_manual/DRM132.pdf .

I've found a zip file associated to this doc which is:

    http://cache.nxp.com/files/soft_dev_tools/software_tools/reference_design_simulations/DRM132_SW.zip

The zip file includes a folder test_FHRM which is referenced on the pdf file page 30 and linked to CW_FetalMonitor_RevX.

It seems to be the right example.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信