After compile, can the codewarrior add a dll or other file to do some post compile action, for example, calculate a CRC based on the s19 file and put this CRC in the specific address area?
解決済! 解決策の投稿を見る。
Hi,
regarding CRC you can go into the CW installation folder (c:\Program Files (x86)\Freescale\CWS12v5.2\Help\pdf\) and look into Build_Tools_Utilities.pdf. There are checksum including principles described there.
Best regards,
Ladislav
Hi,
regarding CRC you can go into the CW installation folder (c:\Program Files (x86)\Freescale\CWS12v5.2\Help\pdf\) and look into Build_Tools_Utilities.pdf. There are checksum including principles described there.
Best regards,
Ladislav
Hi,
just adding my two cents:
Except natively supported CRC calculation by the build tools in Codewarrior for HC12 (as suggested by Lama) it is also possible to run a prebuild/postbuild steps (run a batch script). See the screenshots below:
Stan
Is there a similar feature in the S32DS? I can't find anthing in the help document.
Hi,
S32DS doesn't contain such tools ready for use, but it is possible run post build script - including python ones. Good tool for s-record manipulation are GNU SRecord tools - CRC Checksum Generation with ‘SRecord’ Tools for GNU and Eclipse - GNU Tools - Wiki
Jiri