codewarrior development studio V5.2 (help says 5.9.0) - no option to select MC9S12E128 device, howto install such option?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior development studio V5.2 (help says 5.9.0) - no option to select MC9S12E128 device, howto install such option?

1,344 Views
burtonweakley
Contributor I

I installed codewarrior development studio V5.2 (help says 5.9.0), the nxp website says it is compatible MC9S12E128 device but there is no such device when choosing "Project>>change MCU/Connection", it was however available on codewarrior development studio V5.1. Is there a way to select an MC9S12E128 device?

Labels (1)
0 Kudos
Reply
2 Replies

1,040 Views
trytohelp
NXP Employee
NXP Employee

Hi,

There is a problem with the info provided on the web.

The V5.2 supports only the devices:

    - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96

    - MC9S12G128, MC9S12G96

    - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64

    - MC9S12GN16, MC9S12GN32

    - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128

    - MC9S12XEP100, MC9S12XEP768

    - MC9S12XEQ384, MC9S12XEQ512

    - MC9S12XET256

    - MC9S12XS128, MC9S12XS256, MC9S12XS64

    - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64

For other devices you must use/keep the V5.1.

I've reported the problem (Wednesday) to the webmaster/Product Manager.

The info provided on the web should be clarified.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,040 Views
burtonweakley
Contributor I

Thank you very much.

regards

0 Kudos
Reply