I installed codewarrior development studio V5.2 (help says 5.9.0), the nxp website says it is compatible MC9S12E128 device but there is no such device when choosing "Project>>change MCU/Connection", it was however available on codewarrior development studio V5.1. Is there a way to select an MC9S12E128 device?
Hi,
There is a problem with the info provided on the web.
The V5.2 supports only the devices:
- MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96
- MC9S12G128, MC9S12G96
- MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64
- MC9S12GN16, MC9S12GN32
- MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128
- MC9S12XEP100, MC9S12XEP768
- MC9S12XEQ384, MC9S12XEQ512
- MC9S12XET256
- MC9S12XS128, MC9S12XS256, MC9S12XS64
- MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64
For other devices you must use/keep the V5.1.
I've reported the problem (Wednesday) to the webmaster/Product Manager.
The info provided on the web should be clarified.
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------