change of memory model (CW 5.7  MC9S08RE16)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

change of memory model (CW 5.7  MC9S08RE16)

跳至解决方案
2,405 次查看
stevec
Contributor III
I inadvertantly set my memory model to TINY when I started the project a while back and now need to set it to SMALL. I set the assembler and compiler options under Standard Settings to SMALL (-Ms) and now get a link error L1401:"Incompatible memory model: TINY in previous file ASSERT.C.o (ansitis.lib) and SMALL in (MC9S08RE16.C.o)". Have I missed something out?

Regards,

Steve
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,138 次查看
stanish
NXP Employee
NXP Employee
Hi Stevec,

you have to replace the ansi library since the one you are usnig in the project refers to TINY memory model.
The library has to match with project memory model otherwise it's not possible to link them together.
I'd suggest you to replace file ansitis.lib by ansiis.lib.

The Libs are located here by default:
"<CodeWarrior home directory>\lib\HC08c\lib\*.lib"

For more information about the available ansi libraries I'd suugest you to see:
"<CodeWarrior home directory>\lib\HC08c\readme.txt"

Stanish

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,139 次查看
stanish
NXP Employee
NXP Employee
Hi Stevec,

you have to replace the ansi library since the one you are usnig in the project refers to TINY memory model.
The library has to match with project memory model otherwise it's not possible to link them together.
I'd suggest you to replace file ansitis.lib by ansiis.lib.

The Libs are located here by default:
"<CodeWarrior home directory>\lib\HC08c\lib\*.lib"

For more information about the available ansi libraries I'd suugest you to see:
"<CodeWarrior home directory>\lib\HC08c\readme.txt"

Stanish

0 项奖励
回复