can't update EEprom variable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

can't update EEprom variable

跳至解决方案
1,621 次查看
mikey1
Contributor III
I am using 9s12x512dp processor with CW 4.5.  I am running in large model mode and using Processor Expert to provide the SetWord function.  I have one application that the function works and a very similar application where I fail to update the EEprom.  In the failure case in the WriteWord function after the write to EEprom, it does a read to make sure that the write happened (shown in red in the following code).  the contents of the EEprom remain at 0xFFFF and the function returns an error.
static byte WriteWord(stateMem_TAddress AddrRow,word Data16)
{
  if (ESTAT_CBEIF == 0) {              /* Is command buffer full ? */
    return ERR_BUSY;                   /* If yes then error */
  }
  /* ESTAT: PVIOL=1,ACCERR=1 */
  ESTAT = 48;                          /* Clear error flags */
  *(AddrRow) = Data16;                 /* Array address and program data */
  /* ECMD: ??=0,CMDB=32 */
  ECMD = 32;                           /* Word program command */
  ESTAT_CBEIF = 1;                     /* Clear flag command buffer empty */
  if ((ESTAT_PVIOL == 1)||(ESTAT_ACCERR == 1)) { /* Is protection violation or acces error detected ? */
    return ERR_NOTAVAIL;               /* If yes then error */
  }
  while ((ESTAT & 0xC0) != 0xC0) {}    /* Wait for command completition */
  if (*(AddrRow) != Data16) {          /* Was attempt to write data to the given address errorneous? */
    return ERR_VALUE;                  /* If yes then error */
  }
  return ERR_OK;                       /* OK */
}
What should I look for in differences to see why the one application fails?
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
955 次查看
mikey1
Contributor III
I'm Bad.  I had inadvertenlty commented out the initialization of the the 9s12x register.  Blow this thread

在原帖中查看解决方案

0 项奖励
回复
1 回复
956 次查看
mikey1
Contributor III
I'm Bad.  I had inadvertenlty commented out the initialization of the the 9s12x register.  Blow this thread
0 项奖励
回复