can CW6.3 can be used for the development on MK10DX256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can CW6.3 can be used for the development on MK10DX256

Jump to solution
1,499 Views
manishgirase
Contributor I

Can I use CW6.3 fot MK10DX256 microcontroller

Labels (1)
0 Kudos
Reply
1 Solution
1,233 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Manish,

Sorry the CW6.3 doesn't support kinetis series chips , so we can not develop MK10DX256 microcontroller

on it .

You can use CWv10.6 or KDS , the KDS IDE is free.

If you want use  CW10.6, please refer to this thread to download and install :

New CodeWarrior for MCU v10.6.4 available

If you want to use KDS v3.2 ,please refer to this thread to download and install :

New Kinetis Design Studio v3.2.0 available

Hope it helps you !


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,234 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Manish,

Sorry the CW6.3 doesn't support kinetis series chips , so we can not develop MK10DX256 microcontroller

on it .

You can use CWv10.6 or KDS , the KDS IDE is free.

If you want use  CW10.6, please refer to this thread to download and install :

New CodeWarrior for MCU v10.6.4 available

If you want to use KDS v3.2 ,please refer to this thread to download and install :

New Kinetis Design Studio v3.2.0 available

Hope it helps you !


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply