Hello ,
i am using CW10.5, Coldfire MCF54415 with P&E Multilink BDM.
i am using External Flash S70GL02GS from spansion.
when i try to flash Program this external chip i got this log and it keeps on Executing.
Executing download task: C:\Users\kgaur\Documents\MySVN\ECU_Code\DDR2_Bareboard\ECU_Bareboard\ECU.tcl
cmdwin::fl::target -lc ECU_Bareboard_RAM_PnE U-MultiLink
thread break: Stopped, 0x0, 0x0, cpu68K, ECU_Bareboard.elf (state, tid, pid, cpu, target)
cmdwin::fl::target -b 0x40000000 0x4000000
cmdwin::fl::target -v on -l on
cmdwin::fl::device -d S70GL02GS11 -o 256Mx16x1 -a 0x0 0xfffffff
cmdwin::fl::image -f C:\Users\kgaur\Documents\MySVN\ECU_Code\DDR2_Bareboard\ECU_Bareboard\RAM\ECU_Bareboard.elf.S19 -t Auto Detect
-re on -r 0x0 0xfffffff -oe off
cmdwin::fl::erase image
Beginning Operation ...
-------------------------
log: Trying auto-detect...
Auto-detection is successful.
File is of type Motorola S-Record Format.
log: Using Algorithm: amd16x1.elf
log:
log:
log: ======================================================================
log: === Target Configuration Settings
log: === Launch Configuration: ECU_Bareboard_RAM_PnE U-MultiLink
log: ======================================================================
log: Connecting ...
Performing target initialization ...
log: Connected ...
log:
log: ======================================================================
log: === Execute: Erase
log: === Timestamp: Fri Mar 14 09:06:52 2014
log: === Flash Device: S70GL02GS11
log: === Flash Organization: 256Mx16x1
log: === Flash Mem Start Addr: 0x00000000
log: === Flash Mem End Addr: 0x0FFFFFFF
log: ======================================================================
Downloading Flash Device Driver ...
log: Loading Flash Device Driver at: 0x40000000
log: Flash Driver Buffer is at: 0x40001800
log: Flash Driver Buffer Size is: 0x03FFE800
log:
log: Writing the Address
log: Writing the address of the sector list
log: Clearing the status
log: Setting up Registers
log: Commanding target to run
Reading flash ID ...
log: Reading init return status
log: Done
log:
log: Initialization Command Succeeded
log: Writing Erase Function Code
log: Writing the Address
log: Writing the Number of Sectors
log: Writing the address of the sector list
log: Writing the sector list
Erasing Sector 0x00000000 to 0x0001FFFF
log: Clearing the status
log: Setting up Registers
log: Commanding target to run
Erasing ...
log: Reading erase return status
log: Done
Erase Command Succeeded
log: Timestamp: Fri Mar 14 09:06:56 2014
cmdwin::fl::write
Beginning Operation ...
-------------------------
Using restricted address range 0x00000000 to 0x0FFFFFFF
Programming file C:\Users\kgaur\Documents\MySVN\ECU_Code\DDR2_Bareboard\ECU_Bareboard\RAM\ECU_Bareboard.elf.S19
log: Trying auto-detect...
Auto-detection is successful.
File is of type Motorola S-Record Format.
log: Using Algorithm: amd16x1.elf
thread break: Stopped, 0x0, 0x0, cpu68K, ECU_Bareboard.elf (state, tid, pid, cpu, target)
log:
log: ======================================================================
log: === Execute: Program
log: === Timestamp: Fri Mar 14 09:06:56 2014
log: === Flash Device: S70GL02GS11
log: === Flash Organization: 256Mx16x1
log: === Flash Mem Start Addr: 0x00000000
log: === Flash Mem End Addr: 0x0FFFFFFF
log: ======================================================================
Downloading Flash Device Driver ...
log: Loading Flash Device Driver at: 0x40000000
log: Flash Driver Buffer is at: 0x40001800
log: Flash Driver Buffer Size is: 0x03FFE800
log:
log: Writing the Address
log: Writing the address of the sector list
log: Clearing the status
log: Setting up Registers
log: Commanding target to run
Reading flash ID ...
log: Reading init return status
log: Done
log:
log: Initialization Command Succeeded
log: Trying auto-detect...
Auto-detection is successful.
File is of type Motorola S-Record Format.
Downloading 0x00000BF0 bytes to be programmed at 0x00000000
log: Programming 0x00000000 bytes of Target Memory at 0x00000000
log: Writing Program Function Code
log: Writing the Address
log: Writing the Size
log: Writing the address of the buffer
log: Clearing the status
log: Setting up Registers
log: Commanding target to run
Executing program ....
Executing program .....
Executing program ......
Can anyone please help in this problem which i highlighted in the Red color.
All the Operations Such as Erase , blank check are performed with success as seen in the log.
please help, thanks in advance.
Regards,
Kunal Gaur
Hello Kunal,
there are 2 ways to flash the application:
- via the debugger,
- via the Flash file to Target.
do you have the same problem with 2 flash processes?
http://mcuoneclipse.com/2012/04/30/flashing-with-a-button-and-a-magic-wand/
Regards
Pascal