Why does CW 10.4 attempt to compile a .c file not in source directory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why does CW 10.4 attempt to compile a .c file not in source directory

2,861 次查看
leonmcnutt
Contributor I


I have a construction file that just happens to have an .c extenstion which I #include in my source .c file. My source units compile correctly, however the IDE  attempts to compile my construction file too which stops the build.  I changed the extension of the construction file (.cw2) and I get my static library built. Why  is the IDE attempting to build with .c files outside of the source directory?

标签 (1)
0 项奖励
回复
3 回复数

2,767 次查看
stanish
NXP Employee
NXP Employee

Hello Leon,

The automatic CodeWarrior Makefile generator uses all the files with source file extension within project directory to build regardless of sub-folder where a file is placed.

So if your .c file you are including is not placed completely outside the project directory it will be compiled by default.

However you can explicitly exclude the file from build to avoid compilation of the file. (Click Right on the file -> "Resource Configuration" -> "Exclude from Build..." )

Make sure the include path  to the file is set in the compiler input settings/ Includes path settings.

Stanislav

0 项奖励
回复

2,766 次查看
leonmcnutt
Contributor I

Stanislav,

Thanks for the help!

0 项奖励
回复

2,766 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

don't quite understand your situation. can you please upload your project to showcase the problem?

0 项奖励
回复